Hello,
is there any source code related to the ADS1675? I could find different threads but non with the source code. May someone can email me?
One technical question in addition: is the vhdl implementation alywas with two clock domains, that SCLK is the first clock domain to clock the input signals from the adc or is it also possible to implement only with the internal clock and if so, how fast it needs to be?
Thanks,
Kind regards
Julian Bauer