Hi
My customer is developing a 5-channel device using five AFE4410s.
He pre-produced 10 equipment.
However, the deviation between each channel of the AFE4410 occurs more than 20% and inconsistent.
1. Like TI EVM in the circuit, can adding a Common Mode choke between the AFE4410 and PD help decrement deviation?
2. In the previous circuit review, there was a mention to add Common Mode Choke. Why should I add it?
3. Is it advantageous to locate the AFE4410 close to which of LD (light emitting part) and PD (light receiving part)?
4. Is it advantageous to locate Common Mode choke close to which of AFE4410 and PD?
thanks.
regards.