Other Parts Discussed in Thread: ADS1282, LM27762, TPS54061, ADS8900B
Hi,
I am in search of a precision ADC and came across ADS1278 and ADS1282. My input signal is a true bipolar signal with a low frequency of less than 50 Hz. My objective is to get highest noise free resolution. Comparing both ADCs following key points are observed.
ADS1278 is having an SNR of 111dB at a throughput of 52KSPS when operated in high resolution mode which corresponds to an ENOB of 18.14 bits (Since SINAD is not given datasheet, I have taken SNR = 6.02 x ENOB + 1.76). Oversampling theorem says for every 4 times the sampling and averaging, 1 additional ENOB is gained. So if my required throughput is 1 KSPS, My OSR of ADC output (different from internal Sigma delta OSR) is 52, which corresponds to an ENOB of 2.85. Thus the total ENOB is 18.14 + 2.85 = 20.99 bits. Please correct me if wrong.
For ADS1282, at a throughput of 1 KSPS and PGA =1, the SNR is 124 dB equivalent to 20.30 bits.
Which ADC is the best among both with respect to noise free resolution.
Thanks and Regards
Karthik R