Other Parts Discussed in Thread: PROFIBUS, ,
We want to use both HART and profibus /Fieldbus with DAC8742H. As per my understanding only below hardware changes are required to use both protocols. Please confirm.
|
HART |
Profibus/Field Bus |
1 |
Requires parallel capacitance of 5-22 nF in MOD OUT pin |
Requires parallel capacitance of 0-100 pF in MOD OUT pin |
2 |
If using the internal band-pass filter, connect 680 pF to MOD_INF pin |
If using the internal band-pass filter, connect 120 pF to MOD_INF pin |
3 |
External Clock 3.6864MHz/1.2288MHz |
External Clock 4MHz |
Please let me know if any other hardware circuit required to use both protocols.