This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5296A: Single Ended signal

Part Number: ADS5296A


Hello Team,

Can I use a single-ended signal as input in the device ADS5296A? If ok, how should I do for INx_n?

Thanks in advance.

Regards,


Renan

  • Hi,

    Thanks for using ADS5296A device.

    you can refer to our user's guide page 56 to page 59.

    ADS5296A User's Guide: slau537


    if you don't want to keep INN_n pin

    at least to connect these pins to VCM pin

    please refer to the ADS5296A datasheet page 76 figure 77

    However in this case since the input signal is not differential

    its noise performance won't be as good as differential input signals.

    Thank you!