Part Number: ADS54J40EVM
Hi
I am looking for a way to automatically load configuration to the ADS54J40EVM by writing my own code and without opening the ADS54Jxx GUI.
Thanks,
Yaron
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS54J40EVM
Hi
I am looking for a way to automatically load configuration to the ADS54J40EVM by writing my own code and without opening the ADS54Jxx GUI.
Thanks,
Yaron
Yaron,
If you have access to FMC pins C30, C31, C34, and D35, you could remove U14 and U6, and connect wires from TP13-TP16 to the pads of U6. This would provide a connection for the four SPI lines to be made between the FMC and the ADC. If those FMC pins are not available to use, you would have to interface to whatever you plan on using to create the SPI signals with the test points, and the test points wired to the pads of removed U6.You would still have to use the GUI for the LMK though.
Regards,
Jim