This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1262: Start and Reset Pins

Part Number: ADS1262

Hi Team,

 Our customer is using ADS1262 on their application and they do not intend to use the Start pin as their start command could be sent using SPI commands. The same goes with its reset pin. What would be the proper way to connect Start and Reset pins if they were unused?


Thanks in advance!


Kind Regards,

Jejomar

  • Hi Jejomar,

    If the commands are used to control the ADC's conversion, it's recommended to keep the START pin low to avoid possible contentions between the START pin and the commands.

    If the /RESET pin is not used, please pull it up to the DVDD with a resistor.

    Best Regards,

    Dale