Hi Team,
Posting on behalf of our customer. They intend to operate ADS6125 in parallel CMOS but the datasheet apparently lacks information on the reason the external clock is preferred to use over CLKOUT at DRVDD < 2.2V. Currently they are using CLKOUT and operating at DRVDD=1.8V. They've encountered some noises which is quite expected to some extent but they'd like to know the main factors that contributes these noises.
Are the rising edges not fast enough being a concern? Too low voltage?
Would really appreciate your inputs. Thanks!
Kind Regards,
Jejomar