Part Number: ADS131A02
Other Parts Discussed in Thread: ADS131A04
Hello,
I have a question for ADS131A02.
ADS131A02 SPI has two different modes which are Fixed-Frame mode and Dynamic Frame mode.
Usually the host MCU knows which mode ADS131A02 is in because the MCU controls the mode.
But if the MCU goes out of control because of noise or S/W bugs etc, the MCU don’t know what mode the ADS131A02 is.
In that case, MCU don’t know which mode it should use for the SPI communication.
So the question is that is there any good way to send reset command correctly to ADS131A02 even if the MCU doesn’t know which mode ADS131A02 is?
Regards,
Oba