This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38J84: DAC PLL Configurations

Part Number: DAC38J84

Hi 

I want to use DAC PLL in my application.

My Requirement is

SERDES RATE : 6.25 Gbps

DAC Interpolation : x8

Sampling Rate : 2500 MHz

My Configurations are

DAC Input Clock : 312.5 MHz

DAC Output Clock : 2500 MHz

JESD Clock : 312.5 MHz

SERDES Clock : 6250 MHz

 

 

Are My configurations Correct ?? ( (I have doubt regarding SERDES Clock)

 

I have tried multiple configurations, but I am unable to lock the DAC PLL

Can you help me with the configurations ??

 

 

I have tried this 

  • Hi 

    Please find the attachment of my configuration file for x8 Interpolation without DAC PLL.

    dac_write 0x0    0x0 
    dac_write 0x0    0x1 
    dac_write 0x0    0x218
    dac_write 0x1    0x3
    dac_write 0x2    0x2082
    dac_write 0x3    0xA300
    dac_write 0x4    0xF0F0
    dac_write 0x5    0xFF07
    dac_write 0x6    0xFFFF
    dac_write 0x7    0x3100
    dac_write 0x8    0x0
    dac_write 0x9    0x0
    dac_write 0xA    0x0
    dac_write 0xB    0x0
    dac_write 0xC    0x400
    dac_write 0xD    0x400
    dac_write 0xE    0x400
    dac_write 0xF    0x400
    dac_write 0x10   0x0
    dac_write 0x11   0x0
    dac_write 0x12   0x0
    dac_write 0x13   0x0
    dac_write 0x14   0x0
    dac_write 0x15   0x0
    dac_write 0x16   0x0
    dac_write 0x17   0x0
    dac_write 0x18   0x0
    dac_write 0x19   0x0
    dac_write 0x1A   0x20
    dac_write 0x1B   0x0
    dac_write 0x1E   0x9999
    dac_write 0x1F   0x9980
    dac_write 0x20   0x8008
    dac_write 0x22   0x1B1B
    dac_write 0x23   0x1FF
    dac_write 0x24   0x20
    dac_write 0x25   0x4000
    dac_write 0x26   0x0
    dac_write 0x2D   0x1
    dac_write 0x2E   0xFFFF
    dac_write 0x2F   0x4
    dac_write 0x30   0x0
    dac_write 0x31   0x1000
    dac_write 0x32   0x0
    dac_write 0x33   0x0
    dac_write 0x34   0x0
    dac_write 0x3B   0x1800
    dac_write 0x3C   0x228
    dac_write 0x3D   0x88
    dac_write 0x3E   0x108
    dac_write 0x3F   0x0
    dac_write 0x46   0x1882
    dac_write 0x47   0x1C8
    dac_write 0x48   0x3143
    dac_write 0x49   0x0
    dac_write 0x4A   0xF1E
    dac_write 0x4B   0xF01
    dac_write 0x4C   0x1F03
    dac_write 0x4D   0x800
    dac_write 0x4E   0xF0F
    dac_write 0x4F   0x1C61
    dac_write 0x50   0x0
    dac_write 0x51   0xDC
    dac_write 0x52   0xFF
    dac_write 0x53   0x0
    dac_write 0x54   0xFC
    dac_write 0x55   0xFF
    dac_write 0x56   0x0
    dac_write 0x57   0xFF
    dac_write 0x58   0xFF
    dac_write 0x59   0x0
    dac_write 0x5A   0xFF
    dac_write 0x5B   0xFF
    dac_write 0x5C   0x1133
    dac_write 0x5E   0x0
    dac_write 0x5F   0x3210
    dac_write 0x60   0x5764
    dac_write 0x61   0x211
    dac_write 0x64   0x1
    dac_write 0x65   0x1
    dac_write 0x66   0x1
    dac_write 0x67   0x1
    dac_write 0x68   0x7709
    dac_write 0x69   0x0
    dac_write 0x6A   0x0
    dac_write 0x6B   0xBD07
    dac_write 0x6C   0x7
    dac_write 0x6D   0x90
    dac_write 0x6E   0x0
    dac_write 0x6F   0x0
    dac_write 0x70   0x0
    dac_write 0x71   0x0
    dac_write 0x72   0x0
    dac_write 0x73   0x0
    dac_write 0x74   0x0
    dac_write 0x75   0x0
    dac_write 0x76   0x0
    dac_write 0x77   0x0
    dac_write 0x78   0x0
    dac_write 0x79   0x0
    dac_write 0x7A   0x0
    dac_write 0x7B   0x0
    dac_write 0x7C   0x0
    dac_write 0x7D   0x0
    dac_write 0x3B   0x1800
    dac_write 0x25   0x6000
    dac_write 0x3C   0x228
    dac_write 0x3C   0x28
    dac_write 0x3E   0x128
    dac_write 0x4D   0x300
    dac_write 0x4D   0x300
    dac_write 0x4E   0xF0F
    dac_write 0x0    0x418
    

     

    Now to use the DAC PLL and SERDES PLL, I Have added some more configurations to it

     

    0x02 0x2082 #config2
    0x1A 0x0000 #config26
    0x23 0x0000 #config35
    0x25 0x6000 #config37 Div8
    0x31 0x6408 #config49
    0x32 0x0F00 #config50 Prescalar = 2, M divider = 16
    0x33 0x4D84 #config51 pll_VCO_Sel = 0, pll_VCO = 38 ,PLL_VCO_itune = 11,
    0x3B 0xF100 #config59 SERDES Clk = Pll Clk, Divide Down value = 16
    0x3C 0x82A0 #config60 VRANGE = 1, MPY = 20 (Doubt about MPY for SERDES RATE of 6.25 Gbps)
    0x3E 0x0040 #config62 RATE = QUARTER

    Please verify these configurations

    PLL is not getting locked even with these configurations

    Is there any understanding difference ??

    Please help me out

     

  • Pavan,

    The serdes clock should be 3.125G. The rate = half, MPY = 5, M divider = 8, N divider = 1, pre-scalor = 2. VCO = 5GHz, PLL tune ~ 28.

    See attached.

    Regards,

    Jim

    PLL_mode_Fs_2500MHz.cfg

  • Hi Jim

    What happens if I configure my SERDES Clock as 6.125G and RATE = QUARTER ??

    Will I get the same Result??

  • 5504.DAC38J84 Clock, PLL and SERDES Configuration.docxPavan,

    You will be out of range for this clock. See attached for more information.

    Regards,

    Jim