Part Number: ADS1235EVM
Dear Sir or Madame,
I am new to the TI Device ADS 1235 EVM and I try to connect a 6-wire strain gauge to the ADS 1235. I stick to the description that is given in the manual but nevertheless the Data Analysis part from the Delta Sigma ADC Evaluation Software is not working with my setup. The wiring is done like several examples in this forum. I connected the Exc +/- to AVDD/EXC+, the Exc - to AVSS/Exc-. The signal + reference voltage is on REFPO, the signal - reference voltage is on REFNO. The output + is on AIN1 and the output - is on AIN0.
The predefined script "Enable bridge - external reference" runs without failures
Correct me if I am wrong but it seems like the basic settings are right and I should get at least a signal when I try to collect and analyse data. When I open the Data Analysis part in the Software it tries to connect to the main client but after 2 or 3 minutes it says: Could not connect to main client and the log shows 10 connection failed attempts befor it times out.
I am not sure if the installation is not 100% right or if something else is missing in the configuration. The register is set up like the example script which i ran before. Could you please tell me how I need to process to get data out of the device?
Thank you in advance
Simon