Part Number: TSW1400EVM
Getting "Frame Clock error in Read DDR to file error" message when downloading the .rbf file generated by the quartus II demo program.
When I compile the quartus II project of TSW1400EVM on TI's official website to generate an rbf file and download it to TSW1400EVM through HSDCPro, it shows that the download is successful, and only LED4 of the 7 LEDs is off. But when I press the Capture button of HSDC Pro, the message "Frame Clock error in Read DDR to file error" is displayed.
It is worth mentioning that when I use HSDC Pro to download the default firmware, it can successfully run and capture AFE5818EVM data. So I don't know if I need to modify the Verilog of the DEMO project to run normally.