Hi Jim,.
I want to have more understanding regarding the calibration of the ADS54J60 for minimizing spurs due to the interleave method.
I read in the data sheet that the only calibration is to overcome temperature changes.
My questions are:
1. Is it the only calibration that is required for the ADS54J60.
2. Do you have other calibrations that we can perform in order to minimize the spurs. If yes then what is the process.
3. If there are other calibration we can perform, what will be the improvement in SINAD, SNR, etc...
Thanks,
Yuval