Part Number: ADS131M04
Hello,
My customer test ADS131M04 and found its phase data varied from time to time with the same condition after using phase calibration.
Could you take a look and suggest why?
Test condition:
Two channels of ADS131M04EVM are feed with the same since signal. Phase calibration of one channel had been written 0x0a (4.092MHz, OSR=128, LP Mode, 16Ksps)
When customer read the data multiple times, they found the phase lagging or leading between the two signal. The following is the two different captured figures.
They have tried with DRDY_SEL=0, 1, OR 2, the phase lagging or leading problem always exists.
B.R
Paul