Part Number: ADC12D800RFRB
Hello
I'm jinseong
I am considering buying adc12d800rfrm. I have some questions.
first. I am looking for a dual ADC, and the desired specification is that the analog input BW is about 2 GHz and the sampling rate is 100MSPS.
The most similar among them is ADC12D800RF. But when I looked at the datasheet, it was confirmed that the minimum sampling rate is 150 MHz in Non-DES Mode. Even if external CLK is applied, does 100 MHZ not
work? if not, can you recommend some devices?
second. When using the adcd12800rfrb board, I know that data capture can be performed using Wave vision 5 software. But I want to use NI Labview's Visa function to drive the adc. So, is it possible to connect
directly to NI Labview through the USB port of the board? Or is there a way to connect the wave vision 5 software and Labview?
Any help would be appreciated.
Thanks & Best regards
Jinsoeng