Part Number: ADS4129
Hi,
I can't detect any output clock. I'm using an lvpecl input. The P of this clock signal side can be seen on the follwing image (which follows the 1.6vpp differential):
-The output clock is just two DC values 0.9V and 1.2V.
-The VCM is ok.
-At the moment I don't have and input signal connected and I'm lacking the closest decoupling capacitors.
-I also tried it at higher frequencies (15MHZ,125MHz).
-I didn't use the spi interface yet.
Am I doing something wrong or did I kill de ADS4129?
Thank you,
Best Regards,
Joao