Part Number: DAC8750
Hello,
after working with the DAC8750 for a while I encountered a problem.
The DAC is in the 4-20mA mode with the Output set to 0x0000 (should be 4 mA) but it's 4.23mA.
If the DAC is below 4 mA, like 3.98mA, I already adjusted the output successfully.
But what can I do if it's over 4mA. I think the Zero Calibration Register cannot reduce the output?
If it's set to 0 the output is above 4mA. If I reduce or increase the value of the Gain/Zero Calibration the output at 0x0000 is still 4.23mA.
Thank you very much