Part Number: ADC32RF45EVM
Other Parts Discussed in Thread: ADC32RF45, LMX2582, LMK04828
Hello sir
We are using ADC32RF45 GUI to polarfire
IN GUI
We have given the following parameters
Nyquist Zone : 1st Nyquist Zone
Internal clk frequency : LMX2582 to ADC i.e. 1536MSPS
We are using Bypass mode of resolution 14 bit
it means LMFS is 8224
In LMK04828 section clk0&clk1 zone divider value i am giving 16, it means refernce clk to FPGA is 192MHZ with data rate 7.68Gbps.
we are giving input to ADC is 150MHZ
In JESD204b section of GUI
chA link layer test mode is k28.5 mixed frequency
we are using jesd204b rx IP in polarfire of subclass1
please suggest me to get the data properly with proper sync and sysref.
Thanks
Roja Veereddy