This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1293: ADS1293 SPI I/O 1.8V level connection question

Part Number: ADS1293


Hi TI team ,

ADS1293 spec mention supply power range as below :

1. Analog Supply Voltage: 2.7 V to 5.5 V 

2. Digital I/O Supply Voltage: 1.65 V to 3.6 V

Please refer block as below , MCU SPI connect to ADS1293 for 1.8V I/O level . Is it workable in this Circuit architecture ?  

  • Hello Wei,

    Yes, the power supply scheme should work fine.

    As mentioned in the datasheet, for analog supply voltage of < 3.6V (3.3V in your case), the digital I/O supply voltage range from 1.65 to 3.3V.

    With I/O supply voltage of 1.8V, there should not be any problem.