Part Number: DAC38RF85
What is the sense of the LCM_SYSREF_OUTSEL bit in the LCMGEN register ?
The description says "Chooses between internal and external SYSREF". What value should be used for a design with an external sysref ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC38RF85
What is the sense of the LCM_SYSREF_OUTSEL bit in the LCMGEN register ?
The description says "Chooses between internal and external SYSREF". What value should be used for a design with an external sysref ?
Hi,
If you are planning to use an external sysref then the LCMGEN function is not needed. This is usually used when trying to use an internal sysref.
The default value of the LCM_SYSREF_OUTSEL bit is "0" and this is for an external sysref.
Regards,
David