Part Number: TSW1400EVM
Hi
In my research project, I want to use the kit:
- TSW1400EVM
- ADS54T01EVM
I don't know if this is the right set. Maybe you can advise me?
The set is to be connected to a PC with Windows or Linux (USB + digital logic signal).
The whole thing is to accomplish the task:
- the computer issues the ENABLE signal (logic signal).
(The TSW1400 module starts saving samples in the memory. As long as ENABLE = 1 the set records subsequent samples in the memory. End of recording when ENABLE = 0 or MEMORY is full.
- after switching ENABLE to LOW the computer downloads the read data via USB
- and this is the end of the cycle, everything starts all over again.
- the computer issues the signal ENABLE = 1 .... again and the cycle repeats.
For each data logging cycle, the memory should "erase" and the recording is performed again.
My questions:
- will it fulfill my needs with this set?
- do I have to use TI software to support TSW1400 and ADS54 ...?
I would like to read the data with my own software. Does TexasInstruments provide a description and API documentation of the driver for these modules?
- what parameters the ENABLE signal must meet (what voltage level, steepness)
- where to connect the ENABLE signal to meet my needs? - to the ADS board or to the TSW?
regards
Wojtek