Part Number: ADS1261
Other Parts Discussed in Thread: ADS1260
Seeking clarification on section 9.4.7.4 of the datasheet. It says:
"To calibrate, apply a positive full-scale calibration voltage to the ADC, wait for the signal to settle, and then send the calibration command".
Should this full-scale calibration voltage should be applied to whichever differential inputs are configured in the INPMUX register? I'd like to use the voltage reference external input (on pins AIN0 and AIN1) as the positive full-scale calibration voltage if possible. If I use the voltage reference is the settling time a non-factor?