Part Number: ADS1292
Tool/software: Code Composer Studio
Hi,
I have a problem using ads1292.
When i read sample using continuous mode, drdy pin of ads state is abnormal.
(interrupt edge is low to high : raising edge)
Does anyone know about these problem?
This is my code.
int main(void)
{
WDT_A_hold(WDT_A_BASE);
init_CS();
init_GPIO();
//GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_PJ, GPIO_PIN2 | GPIO_PIN1 | GPIO_PIN0, GPIO_PRIMARY_MODULE_FUNCTION);
register_mainOperation(main_idle);
__enable_interrupt();
initUart();
initUserPort();
setPowerEnPin(true);
initADS1292();
hal_ads_start();
read_started = 1;
while (1)
{
mainOperation();
if (ads_read_flag)
{
hal_ads_read_sample(ads_buff);
ads_read_flag = 0;
}
}
}
#pragma vector=PORT1_VECTOR
__interrupt void P1_ISR(void)
{
switch (__even_in_range(P1IV, P1IV_P1IFG7))
{
case P1IV_P1IFG1:
ads_read_flag = 1;
break;
case P1IV_P1IFG2:
afe_read_flag = 1;
break;
default:
break;
}
}
- ADS1292 SCLK : 1MHz
- ADS1292 CLK : 2MHz from msp430
And, this is register setting of ads1292.
0x01, //CONFIG1 : 4kSPS for single shot mode 0xF3, //CONFIG2 : enable Lead-off comparator, enable reference buffer, reference 4V 0x10, //LOFF 0x65, //Channel1 //power down 0x65, //Channel2 //gain12 0x25, //RLD_SENS 0x0F, //LOFF_SENS 0x40, //LOFF_STAT 0x02, //RESP1 0x03, //RESP2 0x03 //GPIO
Thanks.
Regards,
Youngjun