Part Number: ADS4149
Hi.
regarding ADS4149:
- In the data sheet pin 23 is marked "reserved". Is it ok if I connect it to GND?
- In my application I will use 4x ADCs, the ADCs are directly connected to the FPGA. What do I need the "Output Clock" for?
- For the input clock, "Figure 121" of the datasheet shows an AC coupling.
I guess you would also need a 100 Ohm termination resistor, is it correct?
Thanks
Fred