Other Parts Discussed in Thread: DAC5675A
Hello,
I considering interface circuit for DAC5662 using OPAMP IC.
Below circuit is current/voltage conversion circuit to convert DAC5662 output current to voltage.
The DAC5662 datasheet prescribes Output volatge compliance range of -1V to +1.25V.
I think that the output voltage of DAC5662 is calculated following formula.
I would like to check if the voltage calculated by the following formula corresponds to the output voltage compliance range.
< formula >
Output voltage of DAC5662 = IOUT1 * R1 + EXREF
(Calculation result: +0.5V to +1.0V voltage swing)
Where
IOUT1: 0mA to 10mA sine wave
R1 : 50ohm
EXREF: +0.5V
Regards,
MESH