Part Number: ADS125H02
Other Parts Discussed in Thread: ADS125H01
Hi all,
How should I to convert a RDATA ( MSB , MID and LSB) in order to read the correct temperature?
From the datasheet equation => Temperature (°C) = [(Temperature Reading (uV) - 120,000)/390 uV/°C]+25 °C
Considering I have set all register right and the gain is 1.
I have to convert the data ( RDATA answer) to decimal and then convert to uV?
Like: data_read * 5 ( +-2.5) / 2 ^24 ( ADC resolution 24 bits). It is right?
It is 120 or 120 thousand I have to subtract?
Other point, the datasheet said that the status0 is optional for the RDATA, but I had to have to set the STATENB = 1 to have a meaningful answer.
Thanks for help me
VTC = (VREF • Code) / (215 • Gain)