Part Number: ADS1235EVM
Other Parts Discussed in Thread: ADS1235, ADS1261
I've been using the ADS1235EVM kit successfully with AC Excitation to a load cell with sense lines connected. I have also been able to run a separate instance of the application with a Thermistor connected without issue. The thermistor wired for a single ended measurement with the VCC connected to the 5V through hole on the board, GND connected to GND on J4 and the Thermistor circuit voltage fed to AIN3/AIN1 pin of J2. If possible I'd like to read both the load cell and the thermistor values from the same evaluation kit simultaneously. I am willing to use AC Excitation for the Thermistor and convert the output to a differential signal if necessary but I haven't seen a way to setup the evaluation kit with two differential inputs. Is it possible to run the ADS1235EVM with a differential and single ended measurement (it doesn't look like it from the data sheet). Alterntatively, can the ADS1235EVM be setup for two, simultaneous differential inputs?
The registor ssttings for the Load Cell configuration are:
[ADS1235 Register Settings]
ID C1
STATUS 04
MODE0 14
MODE1 61
MODE2 C0
MODE3 64
REF 0A
OFCAL0 00
OFCAL1 00
OFCAL2 00
FSCAL0 00
FSCAL1 00
FSCAL2 40
RESERVE0 FF
RESERVE1 00
RESERVE2 00
PGA 00
INPMUX 34
The register settings for the Thermistor are:
[ADS1235 Register Settings]
ID C1
STATUS 00
MODE0 14
MODE1 01
MODE2 00
MODE3 40
REF 05
OFCAL0 00
OFCAL1 00
OFCAL2 00
FSCAL0 00
FSCAL1 00
FSCAL2 40
RESERVE0 FF
RESERVE1 00
RESERVE2 00
PGA 00
INPMUX 4E
Thanks,