Part Number: ADS4245-EP
Hi,
Can you answer following:
1) In the datasheet Figure 4 and Figure 5 has difference:
Figure 4: Odd bits are shown at rising edge of CLKOUTP.
Figure 5: Even bits are shown at rising edge of CLKOUTP.
Which one is true?
2) For data outputs, given th ( hold time) is same for all given frequencies in Table 2, bu setup time gets wider with decreasing frequencies.
Is Hold time are all same (min: 0.33 , typ=0.6 ns) for all frequencies?
We are using the device at 10 MHz. Why doesn't hold time gets wider at lower sampling frequencies?
If the hold time is always 0.33 ns, isnt it a contradiction with center aligned source synchronous data transfer?
Do we need to add a phase shift to the clkout signal in FPGA in order to center the data eye?
Mustafa