Part Number: DAC7551-Q1
DAC Experts,
I'm interested in using the DAC7551-Q1 in an automotive application. The package size and daisy chaining are attractive for my application, but the temperature range is not. From an outsiders perspective it looks like there is a very good chance this is the same die as the 6551 with a different bond out. The 6551 is rated for 125C operation but the 7551 is only rated for 105C, but at the same time the 7551 has a max recommended junction temperature of 150C. What is the story on the temperature range of this part? Is this a limitation due to the package?
Thanks,
Trey