Part Number: ADC12DJ3200EVM
Other Parts Discussed in Thread: LMK04828, LMX2582
We have an application where we would like to use the on-board clocking devices (LMK04828 and LMX2582) with an external oscillator. I see a 10 MHz input (CLKIN0) that seems to be only mentioned in the EVM manual briefly, but I want to ask to see if I can use this instead of connecting the signal generators and modifying the EVM. Is there a way that I can just use an external 10 MHz oscillator with the existing clock circuitry?
Thanks,
Anthony