This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I need your help to explain me if I made a mistake with my Hardware configuration to use two ADS1299
- Did the second CLKSEL should be low to force the ADS to use the external clock give it by the first chip
Please see the follow schematic
Hi Jabrane,
As mentioned, Figure 70(b) in the datasheet shows how to configure the device in a daisy-chain configuration. From your schematic, you are not connecting both the ADS1299 devices in a daisy-chain configuration. Referring to Figure 70(b), the DAISY_IN signal of Device2 is grounded and the DOUT signal is routed to the DAISY_IN pin of Device 1. The daisy-chain data for both devices can then be retrieved from the DOUT pin of Device 1.
If you are not driving both devices with the same CLK externally as shown in Figure 70(b), then it is recommended to use a separate RESET signal for each device for a more robust power-up initialization sequence. If you are using the internal CLK of device 1 to drive the second ADC, then you need to set the CLKSEL pin of device 2 to low (external clock). Table 6 on the DS shows how to set the clock for the device. You will also need to set the CLK_EN bit to 1 in the CONFIG1 register to enable the clock to be output in the CLK pin for device 1 (CLKSEL pin set to 1).
Please refer to the same diagram for the remaining signals that can be shared in a daisy-chain configuration.
Thanks.
-TC
I am referring to figure 70(a).
Did the second ADS1299 chip need to be externally CLK driven from the First ADS1299 chip ?
Hi Jabrane,
Figure 70(a) is a standard configuration and not a daisy-chain configuration. You can use device 1 to clock device 2 in this standard configuration as well. The setup I described previously is still valid for this configuration.
Thanks.
-TC
My question is so easy . I can or I should (must) use external clock for the second chip
Thanks,