Part Number: DAC37J82
HI,
We using the DAC37J82 in our design, from the DS the analog output compliance range: min:-0.5V and Max 0.6V.
There is the note :
"
Note that care should be taken not to exceed the compliance voltages at node IOUTP and IOUTN, which would
lead to increased signal distortion.
"
If our signal level is from 0V to 1V with (for example LFM type) on each port IOUTP and IOUTN. I don't see any signal distortion or clipping, why ?
Do you recommend still to be in the range of -0.5V to 0.6V ?
Thanks
Ilia
IOUTP and IOUTN