Part Number: TX7332EVM
Other Parts Discussed in Thread: TX7332
Hello, I am trying to use python file that come with the EVM installation under:TX7332 EVM\Scripts
and I was not able to read or write from the registers using the functions: "write_register" "read_register" in TX7332 EVM.py file,
its seems that I don't use the right PortNumber when I'm initiating the class.
how can I get the right port number of the device and use those function to operate the device?
my source code is very simple and is attached.
import TX7332_EVM
def main():
i = TX7332_EVM.Device_GUI('TX7332_test',float(3370))
i.write_register(1,1,int(255))
reg=i.read_register(1,1)
print (reg)
if __name__ == "__main__":
main()