Hi!
I have a CD drive that outputs 44kHz 16 bit I2S data into the SRC4192 on my board. I want to convert this into 88kHz 24 bit I2S data inside the SRC4192. Under the assumption all settings are correct, is the SRC4192 capable to do so or is it only possible to input 24 bit I2S data into the SRC4192? What would be a workaround to get 24 bit I2S data from the 16 but I2S bitstream if it is not possible with te SRC4192 alone?
Thank you very much
Val