Other Parts Discussed in Thread: TLC3578, TLV2544, TLC2578
Data Sheet: 8625.tlc3578.pdf
Hi
For one of our project design we use TLC2578 to read a analog voltage(10 Volts).
We use PIC18F Controller library to interface the device in SPI.
The following are connection details to host.
Device Pin 1 (SCLK),Pin 3(SDI), Pin 5(SDO) and Pin 8(CS) are connected to host for SPI.
Pin9 (A0) - is connected to Input (One channel only)
Pin19 (REFP) is connected to 4 volts reference.
Pin 24 is not connected.
Please clarify us with the PIN 4(EOC/INT). How to use this in our code.?
Pls post a sample code to understand the sequence.
Thank you.