This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC101C081Q: what is its actual resolution?

Part Number: DAC101C081Q

Hi,

We are powering this DAC from 3.3V and its connections is as follows:

According to the datasheet its a 10-bit DAC but actually its reaching full scale (Vout=3.3V) only when we send 0xFFF (4095). Sending 0x7FF (2047) outputs 1.65V.

It seems this DAC has 12-bit resolution.

Are we missing something here?