Part Number: AMC7823
Hi,
I am aware that if the SS is deactivated (pulled high) before a command is complete, the command is terminated.
However, if I keep the SS low, but stop the SCLK clock (idle state), will I be able to resume the data transmission?
For example, I send a write command, then keep the SS low, and stop the SCLK, while retrieving the write data that should follow the write command. Then send the write data.
Will AMC7823 complete this write operation? or will it terminate the write operation?
Thanks.