Part Number: DAC8801
Hi Team,
According to the first page of the datasheet of DAC8801 the output current (at Vref = +10V) is specified as: 2 mA +/- 20%. A customer wants to confirm if the tolerance value is true.
Regards,
Danilo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC8801
Hi Team,
According to the first page of the datasheet of DAC8801 the output current (at Vref = +10V) is specified as: 2 mA +/- 20%. A customer wants to confirm if the tolerance value is true.
Regards,
Danilo
Hi Danilo,
The current is dictated by the impedance of the R-2R ladder. This device is specified as a 5kohm typical value. Generally, these processes have a +/- 20% tolerance, which is probably where that range comes from. That being said, we do not test the end-to-end impedance of the R-2R ladder, so I do not think it would be wise to assume they are guaranteed. It is best to use MDACs ratiometrically. For example, the RFB resistor is matched to the ladder, so you can use it as a controlled gain.
Thanks,
Paul
Hi Paul,
Thanks a lot for your answer. It really makes sense to use the R-feedback, as it is also suggested in different application-notes. Then to evaluate the accuracy of the resulting DC level, one needs to know how well the value of the R-feedback is tracking the R-values of the R2R-ladder-network. Please advice !
Best regards Ole.
They should match very closely. These processes have very good resistor matching, but the absolute value can vary. I would estimate <1%, but I do not have any characterization data for that.
Thanks,
Paul