Hi there,
What is the load capacitance of the I2C line of DAC43608?
In the system, 2 ICs with IC2 buffers are connected in parallel on the same line, and one of them is DAC43608. So I'd like to know the load capacitance.
Datasheet shows a pin capacitance of 10pF, can I consider this as the I2C line load capacitance?
Best,
Zeming