Hi team,
My customer is using ADS1015 and wondering if the AIN0 input current is over 10mA as datasheet limitation, what would happen?
Would it burn the IC?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer is using ADS1015 and wondering if the AIN0 input current is over 10mA as datasheet limitation, what would happen?
Would it burn the IC?
Thanks.
HI Cynthia,
Yes. Customer had found that PIN burnt out under above condition.
Do you have any failure mode for this scenario?
Thanks.
Hello James,
This is outside the max specs, we do not have a failure mode. But burning out the device does seem like a plausible result.
The customer will need to add protection if this is a case they expect to see.
There is a series of videos on this topic on TI Precision Labs: Electrical Overstress
The videos go over common ways of protection and any discrepancies that could introduce
Regards
Cynthia