This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7128: ADS7128 example code

Part Number: ADS7128

HI Guys

Would we have example code to measure an RMS voltage using analogue input channels in the ADS7128 

Customer was unsuccessful following the datasheet instructions. 

Thanks

Rodney

  • Hello Rodney,

    Unfortunately there is not a direct example for the ADS7128

    But the GUI for the EVM has the capability of exporting the register setting based on the customer configuration. The customer can use the GUI to set the device in the desired configuration, export the register content to achieve this and use that to develop their software. 

    I also suggest using an oscilloscope during debugging. This help provide a visual check to confirm the firmware is behaving as expected 

    If they have further questions, feel free to email 

    Regards

    Cynthia