Dear Forum members.
We are having some trouble with unwanted noise on the input of the ADC.
With absolutely no input signal connected to the input of the ADC only the passive input filter.
we are measuring noise with the oscilloscope (single ended) on Pin30 (INCM)
Please ask if you need further information regarding the implementation or setup used.
Measurements made using small "spring" probe adapter to keep the GND return path as short as possible.
Scope set to 500MHz bandwidth.
Blue trace (CH 3) 30MHz clock input from (Y2) measured on the right hand side of R197. (Scope = DC coupled 1V/Div and +1V offset)
Yellow trace (CH 1) Pin 30 (INCM) measured on TP115. (Scope AC 50mV/Div coupled)
With CH 3 of the ADC switched off via a SPI command the noise reduces considerably.
Could this be a form of ADC "Kick back"
Please see below a screenshot of the input filter arrangement.
Thank you
Regards