This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW1405EVM: LabView Error 7 when trying to connect to ADC3423EVM

Part Number: TSW1405EVM


I’m trying to connect a TSW1405EVM to an ADC3423EVM. The .ini file “ADC342x_2W_12bit” isn’t part of the standard ADC files included with the TSW1405. I copied the file from 1400 Details->ADC files. I’ve included a picture of the folder I copied the .ini file into. When I go to the select ADC dropdown and pick “ADC342x_2W_12bit” or any other option I get Error 7. I’ve included two screenshots of that too. Then it eventually just started giving a different error regarding initializing the ADC (screenshot below). I tried using another computer and removing the R42 resistor and powering the TSW1405 directly with 5V.