Part Number: ADS131M04
Hi
We are using the ADS131M04EVM with a TI c2000 launchpad. We are able to communicate with the device and configure the ADS131M04 registers when using a clock from the DSP and the CLK is applied after the register figuration. But if we try to use the Onboard 8.192MHz Oscillator, the ADC will have CLK all the time but doesn't allow its registers to be configured. Is it possible to configure the ADS131M04's registers while its getting a CLK input?
thanks
Aniruddha