Part Number: DAC7822
Other Parts Discussed in Thread: DAC8822, DAC8805, DAC8820
We are planning to use Dual 12-bit Digital to Analog converter IC part# DAC7822 in our project and are looking for following information which we are not able to get from datasheet:
- This IC is a Two input and Two output DAC which will give two separate outputs based on DAC A#/B selection pin. Can you please let us know what will be the default status of the output when DAC start converting the data?
- When we switch the channel from Channel1 to Channel2 then what will be the status of channel1? Will the data stored in channel A register be cleared automatically or it will hold the previous output result?
- How to clear the Data of channel 1 when we move from channel 1 to channel2.
- Do you have any footprint compatible part with the same features with 16-bit DAC value?
- Can you also please share the register configuration details for the DAC as I am not able to find those details in the datasheet?
Your immediate response on this would be highly appreciated.