Hi,
I am trying to activate the AC Lead-off detection function on ADS1298R chip , I recorded the signal during the Lead-off measurements without any filters in order to validate the measurements process and then noticed strange thing, according to the datasheet the Lead-off signal frequency is fDR/4 and really the frequency of the recorded signal is 125Hz ( the SR of the ADS is 500) bot also the signal contains aliasing Nyquist frequency(in my case 250 Hz) , this phenomenon appears only when I turn on the Lead-off registers. (during normal recording when LEAD-OFF is turned off it is not appeared)
for example:
the recorded signal during Lead-off:
and after the signal filtered by Notch filer (125 Hz) :
as a result , during the Lead-off detection , there is strange fDr/2 frequency signal appear on the recorded signal.
ADS1298R registers Lead-off configuration:
REG_LOFF_0X04, 0x1D
REG_LOFF_SENSP_0X0F, 0xFF
REG_LOFF_SENSN_0X10, 0xFF
I need to know the source of this signal and also to get rid from in order to be able to get accurate Lead-off detection process