Other Parts Discussed in Thread: DAC3283, CDCE62005
Hi,
I am using the TSW3100 to generate a sinewave of 70MHz±20MHz with the DAC3283. The TSW3100 has a inbuilt 100MHz oscillator which limits the operation to 200MSPS. Moreover the DAC3283 has a CDCE which runs on 19.2MHz. I am not sure on how to control the CDCE (mainly VCO) which determines the DAC_Clk, the data rate of TSW3100 as interpolation is to be enabled.
I am planning to operate the TSW3100 at 312MSPS, DAC_Clk to be 624MHz and the frequency should not go to the 2nd zone. Please let me know which configuration would/can be used for achieving this.