Hi,
As per the current sync DAC requirement, We have given 71.5 ohm pullup to P5V0 and 165 ohm pull-down to ground to maintain 50ohm impedance in AFE DAC output (IOUTP/N_A_DAC and IOUTP/N_B_DAC).
In assembled board, Due to this pullup and pulldown resistor the complete 5V power rail impedance become around 50 to 55ohm.
For your information, In our design we have connected this same P5V0 power to other sections as well.
Could you please let us know is this 5V power rail impedance is expected if we connect this power to current sync DAC using 71.5Ohm pull-up resistor?
What is the expected impedance of AFE DAC output pins?
Is this 5V rail impedance is OK to power ON the boards or Is there any solution to increase 5V rail impedance?
***From similar thread***
What is the expected impedance of +3.3VA_DAC and +5VA rails in below configuration,
1. What is the expected impedance of +3.3VA_DAC power rail in EVK.
2. What is the expected impedance of +5VA rails if we make R46, R56, R58 and R68 are DNI and mount R114, R120, R127 and R133 resistors
Please clarify all the points...
Thank you....