Part Number: AFE5809EVM
Other Parts Discussed in Thread: AFE5809, AFE5808,
Hi Team,
I'm posting on behalf of our customer in their question regarding TIDU702:
tidu702.pdf
1. What exactly is required to decimate for a signal starved sonar acquisition? Note: for my application demodulation is NOT desired, but decimation is desired.
- in TIDU702, p 23 indicates that an external trigger is required to trigger the DEMOD block in the AFE5809. But my signals are so low frequency that I demodulation is unnecessary. And Fig 21 seems to indicate that demod can be bypassed.
- is it necessary to test using an external clock, or can we use the eval board’s internal clock to get started?
- what firmware is required to decimate without demodulation?
- “Frame clock error in Read DDR to file” message appears when trying to use AFE5809_16x firmware. I cannot find AFE5808_09_16b firmware in the dropdown
- I can acquire triggered data using AFE5809_14x firmware, although phase appears to be shifted
2. Vref – can we reduce it for signal starved applications?
3. gain validation - please confirm that for AFE5809, 14 bits acquisition, 1 count ~ 2^{-14} V (I compute gain assuming 2^{-14} V/count and do not always realize 54 dB gain when LNA and PGA gains are set to 24 dB and 30 dB, respectively)
Please let me know your inputs.
Thanks,
Jonathan