This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC3174: Channel isolation performance

Part Number: DAC3174


Hello team,

Do you have channel-channel isolation performance data of DAC3174?

If you have it, could you share it with me?

Best regards,

  • Sato-san:

    I do not explicitly have the isolation data for the DAC3174.  However, similar DAC devices achieve isolation performance that is better than 70 dB.  Note, it is difficult to measure this performance on the EVM as the output transmission lines and transformers will typically couple two orders of magnitude worse than the silicon/device itself.

    --RJH